• Registrarse
  • Identificarse

Novedades

Print page

PLCs

Aquí lo tiene usted todo bien claro

Informaciones actuales

2016-04-28 – Mitsubishi Electric's iQ Platform and Standard PLC Open Function Blocks reduce time to market for packaging machines

Mitsubishi Electric will be using a tubular bag machine to demonstrate its packaging machine engineering expertise at Hanover Trade Fair. The trade fair application is based on Mitsubishi Electric's automation iQ Platform. The system uses predefined function blocks especially for packaging machines which can be used to set up control systems including HMIs quickly and easily. The program ...

PLCs

2016-03-22 – Preparing pharmaceutical and medical technology for the future

Production environment requirements in the pharmaceutical and medical technology sectors are very high. Not least, the strict cleanroom criteria present a particular challenge. In order to survive in a highly competitive market, companies also need to make sure that they increase their production effectiveness and minimise costs. Current trends include process optimisation for the purpose of ...

2016-03-15 – Mitsubishi Electric integrates own Factory Automation products to optimise building management processes

The Factory Automation Division of Mitsubishi Electric Europe B.V. has installed an extensive range of building automation and security products in the newly built German Branch in Ratingen. The products and solutions can be used for a variety of applications, for example quantifying, measuring, displaying, recording and monitoring current and voltage flows around the building. All the data ...

2016-03-08 – Mitsubishi Electric anuncia su participación en la Feria BIEMH de Bilbao

Mitsubishi Electric innova en tecnologia de automatización para mejorar para mejorar la competividad de fabricantes de maquinaria. Del 30 de Mayo al 4 de Junio en Bilbao

2015-11-27 – SPS 2015 - Using global experience to make renewable and EFW power plants more efficient

Energy from Waste (EFW) plants around the world rely on automated systems from Mitsubishi Electric to optimise performance and ensure maximum levels of efficiency while also achieving rigorous environmental standards for emissions.

2015-11-27 – SPS IPC DRIVES 2015 - Mitsubishi Electric continues its record of innovation in automation technology

Mitsubishi Electric is presenting several innovations in key automation technologies at the SPS IPC Drives. These cutting edge technologies have been developed to enhance the productivity, efficiency and performance of production plants across all industrial sectors.

2015-11-10 – Preview - The world of automation at SPS IPC Drives

Integrated solutions for manufacturing and production industries are increasingly becoming state-of-the-art. The demand for better quality products, almost immediate availability and more product variants is constantly growing: Traceability, OEE (Overall Equipment Effectiveness), and resource management for example are becoming increasingly important for innovative companies...

2015-11-03 – History and the future both influence the latest automated production innovations of today

Mitsubishi Electric will have many of its key technologies on show at the EMO Exhibition (Milan, Italy, 5-10 October 2015, Hall 3, Stand H18/L17), where experts will also be on hand for discussions and demonstrations.

2014-03-18 – Innovation in Packaging applications with Mitsubishi Electric’s Motion Control technology

Mitsubishi Electric is a world leader in the three principal application areas for servo drives in industrial automation: robotics, CNC and general motion control (GMC). Mitsubishi manufactures its own technologies in all of these fields, something which very few other manufacturers can match. Combining this capability with unmatched service results in control solutions enabling ...

2014-03-12 – IFAT preview - Mitsubishi Electric diseña soluciones especiales de gestión del agua

En este año IFAT - la feria más importante del mundo para la gestión del agua, aguas residuales, residuos y materias primas - Mitsubishi Electric, junto con su filial ME-Automation Projects GmbH (anteriormente KH-Automation Projects), presentará una gama de soluciones innovadoras diseñadas para el mercado del agua. Las dos compañías compartirán stand A5 425/524 en el pabellón 5.

2014-02-06 – Producción en panadería lista para el futuro gracias a la transparencia de los datos

Mitsubishi Electric está cambiando el enfoque a la industria de la panadería con su presentación "El aumento de la productividad a través de la Tecnología de Automatización en la Industria Alimentaria". Stefan Knauf, key account manager de Alimentos y Bebidas, CPG, estudiará las opciones para mejorar la eficiencia...

2013-12-12 – KH-Automation Projects GmbH becomes ME-Automation Projects GmbH

KH-Automation Projects GmbH, which has been part of Mitsubishi Electric Group since mid 2013, is changing its name on 1st January 2014 - subject to completion of the formalities for entry in the Trade Register - to ME-Automation Projects GmbH.

2013-12-12 – Mitsubishi provided a look at its future automation solutions at SPS IPC Drives 2013

At this year's SPS IPC Drives, Mitsubishi Electric provided visitors with a look into the future of its automation solutions. For the first time in Europe, the successors to the globally popular compact MELSEC FX PLC series and the latest generation modular MELSEC iQ Platform were on show, alongside the new GOT2000 series touch screen HMI and the new FR-A800 high-end frequency inverter range.

2013-11-26 – Mitsubishi Electric presenta el nuevo PLC modular MELSEC iQ-R

Mitsubishi Electric ha presentado el nuevo concepto de controlador modular, MELSEC iQ-R, por primera vez en Europa en la feria SPS IPC Drives 2013 en Nuremberg. Comparado con su predecesor, el exitoso MELSEC System Q, el nuevo controlador modular de altas prestaciones reducirá considerablemente los costes de desarrollo así como de mantenimiento y operación. Al mismo tiempo, las prestaciones....

2013-11-26 – Nueva serie MELSEC FX5 de Mitsubishi Electric – la nueva generación de PLCs

El Nuevo MELSEC FX5 es la nueva generación del exitoso PLC que Mitsubishi Electric lanzará al mercado. Se trata del sucesor del avanzado MELSEC FX3, que avanzará drásticamente la productividad de los equipos y reducirá los costes totales de operación así como el consumo energético. La nueva serie de PLC ofrece ventajas significativas sobre sus predecesores y es plenamente compatible con la ...

2013-11-11 – Next Generations – Experience the future live at SPS IPC Drives

At this year's SPS IPC Drives, Mitsubishi Electric will be giving visitors a closer look into the future of its automation solutions. For the first time in Europe, the successors to the compact MELSEC FX PLC series and the modular automation concept MELSEC iQ Platform, the brilliant HMI GOT2000 series and the FR-A800 high-end frequency inverter will be presented.

2013-11-07 – Mitsubishi Electric’s iQ Platform: full automation on one rack

Machine tool manufacturers have been successfully combining Mitsubishi Electric CNC and robot technology in their systems for years and consequently promoting unmanned production. The iQ Platform from Mitsubishi Electric permits not only the seamless combination of CNC and robot CPUs but also of PLC and Motion Control CPUs – an integrated solution that is unique throughout the industry...

2013-10-29 – Mega project uses Mitsubishi Electric controls to improve Sussex coast water quality

One of the most ambitious wastewater treatment projects in Europe, designed to process several towns’ wastewater and improve water quality along the Sussex coast, has been speeded along because of the ease of integration of Mitsubishi Electric control equipment.

2013-07-18 – Mitsubishi Electric presenta el FX3GE

Mitsubishi Electric ha extendido la familia compacta de PLCs MELSEC FX3G con la introducción de una nueva CPU que lleva puerto Ethernet integrado – la FX3GE. Esta llega como adición a los ya disponibles puertos RS422 y USB, además la nueva CPU añade también dos entradas analógicas (0-10V DC o 4-20mA) y una salida analógica (0-10V DC o 4-20mA).

2013-06-19 – Los PLCs de Mitsubishi Electric controlan AGVs en una fabrica de motores

Un importante fabricante de automoción se beneficia de una mayor producción en sus motores gracias a la utilización de vehículos guiados automáticamente (AGV) para transferir componentes a diferentes estaciones en el proceso de montaje. La clave para el diseño y funcionamiento de los AGV son los PLC de la serie MELSEC-L de Mitsubishi Electric.

2013-06-04 – Lanzamiento de la expoción e-F@ctory Alliance en el mundo virtual

La exposición e-F@ctory Alliance es la primera exposición completa que se realiza con nueva plataforma de exhibición virtual de Mitsubishi Electric, y la primera muestra virtual para ofrecer una gran experiencia gráfica y convincente a los visitantes.

2013-04-24 – Mitsubishi Electric y Raima crean un proceso seguro de manipulación de datos

El control y la gestión de un sistema complejo es difícil en cualquier momento. Sin embargo, los usuarios de proceso (por ejemplo agua, petro-química) y las industrias de infraestructura, como el ferrocarril, los aeropuertos o los sistemas de metro subterráneo tiene la complejidad añadida de tener que hacer lo mismo a distancias extremas con la miles de puntos de E/S

2013-04-15 – Eficiencia Energética con Mitsubishi Electric y KH-Automation en WASSER BERLIN 2013

En la feria WASSER BERLIN INTERNATIONAL (23 – 26 Abril 2013), Mitsubishi Electric y KH-Automation mostraron soluciones de automatización para el sector del agua. Las dos compañías se especializan en los sistemas para los sectores del agua, aguas residuales y residuos. Los puntos focales son la eficiencia energética, mantenimiento remoto, mantenimiento preventivo y control de estado.

2013-03-26 – Tendencias de la tecnología de control: ¿hay un futuro para el PLC?

Cambio define el mundo. Los desafíos actuales de la sociedad van des del cambio demográfico hacia una creciente escasez de recursos naturales. La automatización, también está cambiando: las tendencias futuras en la tecnología de control sugieren que la tecnología de control cambiará ... Los expertos de Mitsubishi Electric ya estan ofreciendo soluciones preparadas para el futuro.

2013-03-05 – Líneas inteligentes de transporte alinean quiches en cocción de precisión

En la campaña para reducir los envases y sus residuos resultantes, un constructor de maquinaria especializada ha desarrollado un transportador de cola sin presión para alinear quiches antes de hornear.

2013-02-26 – Cyber seguridad – que viene ahora?

Los incidentes de gravedad con el malware Stuxnet, proporcionaron un oportuno recordatorio de que tenemos que tomar medidas eficaces para proteger los sistemas de control de procesos y de infraestructura de los ataques del ciberespacio. Thomas Lantermann, Business Development Manager Senior en Mitsubishi Electric, analiza donde se encuentran las vulnerabilidades y cómo el problema se agravará

2013-02-13 – Mitsubishi Electric optimiza el tratamiento de aguas residuales y plantas de purificación de Irlanda en un tiempo récord

El objetivo de los operadores de una planta de tratamiento de aguas residuales y cuatro plantas asociadas de purificación en el Este de Irlanda era reducir los costos de operación en curso a través de la modernización. Para ello, la planta fue actualizada mediante la instalación de componentes de automatización de Mitsubishi Electric. Se trataba de tomar los requisitos de rendimiento así como...

2013-02-12 – La Empresa de Producción integrada en 2020

La globalización, la creciente sofisticación del cliente y la escasez de recursos son los desafíos que afronta la industria de procesos, y en 2020 estos serán aún más agudos. Hacer frente a estos retos dependerá de estructuras que permitan la planificación totalmente automatizada, programación dinámica y los procesos totalmente optimizados para controlar los costos de producción.

2013-01-24 – Water industry moves to less data, more information

Regulators are driving the water industry to adopt Whole Life Asset Management, as the best way to ensure overall efficiency, keep prices down and quality up. This has created a need, not for more data but for better information, so the recent ‘Driving Innovations in the Water Industry Conference’ hosted by Mitsubishi Electric Europe B.V.’s, UK Branch looked at how some companies...

2012-12-13 – Mitsubishi Electric Europe improves PLC-based data logging

In the push for increased overall equipment effectiveness (OEE), reduced energy usage, improved traceability, analysis of key performance indicators and more, the vital ingredient is data. Barry Weller, Product Manager-iQ Platform, Automation Systems Division of Mitsubishi Electric Europe’s UK Branch discusses why data logging has become an essential feature of modern production line and why...

2012-12-04 – Mitsubishi Electric presenta su solución en unidades terminales remotas RTUs

Las innovadoras soluciones permiten a los procesos totalmente automatizados ser controlados remotamente, lo que significa la reducción al mínimo del personal empleado. En conexión con esto, Mitsubishi Electric presenta su nueva gama Remote Terminal Units inteligentes (smart RTUs).

2012-10-31 – Datos: seguros al alcance de la mano

Raima y Mitsubishi Electric han extendido su colaboración en e-F@ctory basada en la base de datos Raima RDM y el C Controller basado en la iQ Platform de Mitsubishi Electric, para proporcionar datos seguros directamente a dispositivos mobiles, incluyendo ipads bajo demanda.

2012-01-11 – Mitsubishi Electric’s C CPU opens up the world of automation for easier system development

Systems designers, who prefer the flexibility of PC based control, have previously had to choose between industrial PCs or embedded microcontrollers for their bespoke automation control systems now have a third option: Mitsubishi Electric’s C-language controller.

2011-12-14 – Mitsubishi Electric makes motion control easy with the MELSEC L-Series Simple Motion Module

Mitsubishi Electric has expanded its MELSEC L-Series range of positioning modules with the new Simple Motion Module, enabling advanced motion control functions such as positioning, speed control, torque control, cam control, synchronous control and mark detection to be realised easily with just simple parameter settings and a sequence program accredited to IEC 6M3N-3 standard.

2011-11-24 – Mitsubishi Electric introduce MELSEC L

Mitsubishi Electric ha lanzado el nuevo PLC modular sin rack con altas prestaciones posicionado entre la series MELSEC FX y la plataforma iQ

*Nota: Mitsubishi Electric es la propietaria de todos los derechos sobre los textos y las imágenes. Pueden emplearse libremente siempre que tal empleo sirva de forma unívoca para informar públicamente sobre Mitsubishi Electric o acerca de nuestros productos. Los textos o las imágenes pueden emplearse para otros fines distintos a los indicados sólo con nuestro consentimiento expreso.

Consultas
Contacto
Base de conocimiento
Ayuda

SmartConditionMonitoring – Mantenimiento Predictivo para mejora de la eficiencia
Más